User Activity

Hi,   Due to my mistake, when using the GUI tool to update the firmware, I mistakenly loaded the configuration file into both the PATCH and CONFIG sections. As a result, the chip is not functioning properly and cannot connect to the GUI tool. Is ther...
Hi,I use the STWLC38 for wireless charging.Just set the BPP VOUT to 9V, and other REG is in default value.In test , the output current around 0.6A . (The chip emits a squealing sound)If I want to set the Rx to 15W, which REG I need to set. And I have...
Kudos given to