Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-ISB042V1 in Tx mode

Posted on February 28, 2018 at 09:31Hello,Where could I find the binary file STWLC33_TxMode_RAM_binary.bin need for set the STEVAL-ISB042V1 board in transmitter mode ?The STEVAL-ISB042V1 development board is a dual mode wireless power evaulation boa...

FIT Rate/ MTBF of ST1L08SPUR

I'm using ST1L08SPUR in my project. For reliability analysis I wanted to know FIT rate/MTBF of ST1L08SPUR.Please help me out in this concern.RegardsNidhi P Shetty

NShet by Associate
  • 638 Views
  • 0 replies
  • 0 kudos

STGAP2D isolated half-bridge gate driver: very specific question related to on-chip internal voltages applied to the gate of GOFF NMOS transistors with respect to GNDISO_A/B and their current drain versus gate voltage (internal) characteristic

The reason I need this information is because I would like to use the two internal 'half-bridge' of the STGAP2D gate driver for directly driving a resistive load at ~ 300 mA (more explanation below). In addition, the configuration / topology I am tar...

FDORE by Associate
  • 652 Views
  • 0 replies
  • 0 kudos

It is a question of regulator RHFL 4913.

​It is a question of regulator RHFL 4913.There is a noise graph on the data sheet(DocID10005 Rev17 Figure 37), but there is a peak at 30 kHz.Is RHFL 4913 a switching power supply?If it is not a switching power supply what is the noise of 30 kHz?Thank...

STSPIN250's can I use 3.3V for it's logic pins?

STSPIN250's EN\FAULT and STBY\RESET pins are described as "Logic input 5 V compliant". Does it mean it only supports 5V logic or 3.3V logic will do the job of bringing these pins high?Want to use this device with STM32L496 MCU which is a 3.3 device.

STEVAL-PCC009V2 missing source file for IBUU source code, where to find it? Many trouble with this board and no answer...

Dear all,as stated inside the UM0935, page 8/53, §2.2 it should be on the package also:"The IBU UI tool includes the following items:�? Hardware content:– One board– BOM list– Schematic�? Software content:– DFU firmware– DLL files of the I2C, SPI and...

FF1 by Associate III
  • 798 Views
  • 0 replies
  • 0 kudos

STEVAL-PCC009V2 firmware reflash

Posted on January 08, 2013 at 01:12I have STEVAL-PC009V2 communication board for the L6470 evaluation purposes. I saw some posts found bugs on either communication board or PC software during the evaluation therefore I went to the website and downlo...

VNQ5E160AK-E (new design) vs. VNQ5160 (old design): can current sense pins stay unconnected (and CS_DIS set to GND via 10k resistor), so the old PCB design can be kept?

We are using VNQ5160 in a project, but those chips are now not avalible and we would replace them with VNQ5E160AK-E. Footprint and switching power is the same, the only main difference is in status pins, where older chip has status outputs and new ha...

GMace by Associate
  • 1323 Views
  • 1 replies
  • 0 kudos