cancel
Showing results for 
Search instead for 
Did you mean: 

The diffrence of MC_Library_ProtectedSources files

hankui zhang
Associate II
Posted on July 19, 2017 at 11:39

I noticed there are two lib files in Cortex-M4 core MCU:

MC_Library_ProtectedSources_SD_CM4_CCM_MKD.lib and MC_Library_ProtectedSources_single_drive_CM4_MKD.lib

I can't find any description for the diffrence between them, so I should choice which one in my application?

thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
hankui zhang
Associate II
Posted on July 31, 2017 at 08:43

anyone can help me

Jakob K.
Associate II
Posted on November 25, 2017 at 19:03

The CCM Lib makes use of the Core Coupled Memory, functions are executed from RAM (=significantly decreased critical task execution time). See also AN4296 and UM1080