Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello,I’m trying to design a solar panel charger circuit! There will be 6V, 12V or 12V one solar panel and I need to charge the lithium battery 3.7V. A tricky bit is that when 6V solar panel is used, it needs to charge the battery and the battery wil...
Hi all,for a stepper based application I've to link the frequency that came from a quadrature encoder to the driving speed of a bipolar stepper motor. This board is equipped by a STM32F105RB processor, I've read inside the RM0008 (the reference manua...
Posted on January 24, 2018 at 19:10Hello,Im trying to build the spin3202 6 step firmware packageFor some reason the STSW-SPIN3202 firmware package is missing the pre compiled binaries mentioned in UM2310 section 2.5.2if I then try to compile Keil p...
As shown in the photo, the polarity of this component was reverse mounting in same location of our products.Please tell me whether this part has polarity. It can not be determined by body marking.Best Regards,Enomoto
We have been trialing some of this energy monitoring eval boards to develop an OEM application. To cross-check and validate test results we need to perform some calculations for which I need this transfer ratio value for sensitivity etc. Please help....
Dear Sirs,I've to develop a microstepping application (1/128) and I'm thinking about the L6480 stepper driver. My question is how to correctly start in developing with this driver. Actually I've bougth a EVAL6480H (R1.1) eval board, on this there are...
Does anyone help me to get application note for RHFL7913. and also block diagram for RHFL7913 SMD5C package.Regards,Swamy M.