Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Noise (click) problems while driving BLDC motor by using SPIN3202

Hi all, after many hours of tuning and trials I finally got my new BLDC motor running. It's a 36V, 180W rated power, Nominal current 6.8A.I am using FOC with 3 Hall sensors and single shunt. Problem I am facing is, quite often motor makes strange noi...

PaulQ by Associate III
  • 1125 Views
  • 0 replies
  • 0 kudos

L6470 / L6472 VREG line question

Hello, I am designing the system with both L6470PD and L6472PD stepper drivers. Since my system is operating on 3.3V (MCU is STM32F103 ) I have tight the VReg with VDD line as suggested. The problem which I am facing is following. I supply the drive...

L6480H stall detection does not work. What should I do?

Hi everyone!I want to use the ST EVAL6480H board to control a stepper motor but I get stuck with the stall detection feature of the chip. My problem is that it always generates stall (step loss). I have tried it with different configurations and wit...

DDely.1 by Associate
  • 666 Views
  • 0 replies
  • 0 kudos

Multiple L6470PD via daisy chain.

Hello FolksThe L6470 datasheet (see snapshots provided by Jacek) clearly says that Vreg should be connected to VDD, as they are not connected internally. Further, VDD should have 10uF Cap to work properly.Surprisingly, the X-NUCLEO-IHM02A1, which has...

0690X00000BvwHXQAZ.png
JSing.11 by Associate II
  • 1009 Views
  • 0 replies
  • 0 kudos

When STC3115 power gauge depicts an incorrect SoC value (remaining charge in battery), showing a value less than the correct one, may STC3115 discharge calculus be artificially forced to a lower discharge rate by changing the declared value of Rsense?

Although for 3 different batteries we managed to get the expected SoC and duration of battery discharge, we are facing difficulties in getting the expected discharge time for a fourth battery type. We followed the same procedure used to characterize ...