Skip to main content
NA.1067
Visitor II
November 12, 2019
Question

Why is the voltage high?

  • November 12, 2019
  • 0 replies
  • 461 views

I’ve bought 1000+ L7805CP voltage regulators. On all the data sheets it say there is a +-10% voltage tolerance yet the voltage I’m getting is +55%. It says it’s input voltage range is 35v - 7v and its output is a nominal 5v (4.5-5.5v) yet I’m getting 7.85vdc. My power source is a 28.8v battery. Is this just a faulty batch?

thanks.

This topic has been closed for replies.