Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to munt and cool D2PAK IGBT in power bridge

I want to use  STGB8NC60KDT4 IGBT, 15 A 600 V, 3-Pin D2PAK (TO-263)in a motor controlpower bridge, The bridge will be running at 300VDC and about 3-5 amps. At this power there will be 6-12 watts dissipated in the IGBT.I would like to cool them by scr...

shorai by Associate III
  • 1051 Views
  • 2 replies
  • 0 kudos

SG3525 technology

hi i use your product SG3525 for Solar inverter (input-dc 12v , out put -110v ac 60hz​could you recommend me how to use transformer for step up tr(T1)how to calculate core size, coil thickness and turns for primary, and secondaryalso i hope to know i...

HJeon.2 by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

I have problems to setup a communication over I2C with my MCU and a STWLC33 on a STWLC33JRF eval board. The data sheet of the STWLC33 has errors. See details.

Chapter 8.5 says write the register value as two bytes (Low and High), but all pictures and descriptions later sends only one byte for the register value. Whats correct?If I send START ADR(WRITE) REG START ADR(READ) VALUE STOP the ADR byte is acknowl...

DZwir.1 by Associate
  • 608 Views
  • 0 replies
  • 0 kudos