Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to I sync two SPV1040 solar charger ICs connected in parallel so that both of them have the exact voltage set point?

I am using 2 SPV1040 that are controlling 1 solar panel per chip. With that said, I am using a super cap with no battery and when the super cap is discharged the two ICs work in unison to charge the Super cap to the voltage set point. Once that is co...

PTher.1 by Associate
  • 1194 Views
  • 2 replies
  • 0 kudos

L6470 absolute position counter

Hi all,I have questions about L6470 absolute position counter:Can it be used reliably to count how many steps (or micro steps) the motor actually spins? For example, when at ABS_POS 0, if executing GoTo_DIR(1, 25600) (1/128 micro step mode), does it ...

MT.1 by Associate
  • 1496 Views
  • 2 replies
  • 0 kudos

BLDC simulink file and source code.

Hello~ I am program stm32f302r8 for bldc motor control. Does any ones has the file and source code like below? Luenberger state observer Rotor position estimation simulink file, source code for maximum torque per ampere, feed-forward current regulati...

Vnguy.1 by Associate II
  • 865 Views
  • 0 replies
  • 0 kudos

Hello. I'm trying to find the switching losses for the IGBT "STGB30H60DFB". I found different Methods. Details in Detail-Window... Any help?

Switching losses:1. P = f * (Eon + Eoff) --> P = 32000 Hz * (383 uJ + 293uJ) = 21,632 W2. Pswon = 0,5 * Un * In * Füein * tr/T --> P = 0,5 * 325 V * 8,88 A * 1,2 * 14,6 ns / (1/32000 Hz) = 0,809 W Pswoff = 0,5 * Un * In * Füein * tr/T --> P = 0,5 ...

POffe.1 by Associate
  • 616 Views
  • 0 replies
  • 0 kudos