Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Datasheet by diode

Could someone tell me what type of diode I have? I can't find any data.L X GP128I appreciate your help.

Imagen de WhatsApp 2025-08-19 a las 10.00.47_07913828.jpg

Resolved! STCP202000CFP's Rth(j-c) definition

Now I start to use STPS202000CFP and try to estimate junction temperature. Then in datasheet, ST defines Rth(j-c). Question1 : where is "c(case?)" point in this discrete device, center of case?. Question 2: Does Onsemi have Rth(j-a) for this device ?

skkmtshr by Associate
  • 1074 Views
  • 1 replies
  • 0 kudos

HVLED007 in PSR

Hi,I am using HVLED007 in my 80V, 45W SMPS (Input voltage range 160V-300V). Is it possible for the IC to operate in primary side regulation mode instead of the conventional opto-coupler-based secondary side control? Unlike other ICs, I cannot see an ...

Spice98 by Associate
  • 1232 Views
  • 0 replies
  • 0 kudos

Resolved! LD1086DT33TR and ESR

I plan to use the LD1086DT33TR LDO to output 3.3V with an input voltage of 5V. However, I am not aware of the requirements for the ESR (Equivalent Series Resistance) of the output filter capacitor for the LD1086DT33TR, and this parameter is not menti...

STSPIN948 and stepper motor

Hi,does anyone in the world have used a STSPIN948 with a stepper motor?I'm having many problems, also because of lack of documentation and examples.I need to control a NEMA 23 motor, but if it turns slowly it works, over 2 turn per second it hangs.I ...

giuseppe by Associate II
  • 422 Views
  • 1 replies
  • 0 kudos

Question re: BMS control and Inverter control

Hi,I was hoping someone may be able to point me in the right direction for two projects I am looking to research:1.) BMS - to what extent is there a mature ecosystem and codebase for scalable battery management - not only for varying call capacities,...

DGerkin by Associate
  • 570 Views
  • 0 replies
  • 0 kudos

Resolved! Stm32 Nucleo 767zi power on issue at 12V Vin.

Hi!I have an issue with stm32 Nucleo F767zi power setup.When I power up the stm32 Nucleo F767zi on 12V, the regulator ic and the controller chip heats up. Why?I have also changed the JP3 jumper to (Vin-5V) option. And the JP1 jumper is off.What's the...