STPSC10H12G-TR Replacement
Hello,STPSC10H12G-TR is used in our projects, it's NRND and may be going to EOL.Do you have recommended replacement for this part? Thanks!
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hello,STPSC10H12G-TR is used in our projects, it's NRND and may be going to EOL.Do you have recommended replacement for this part? Thanks!
Hello,I'm currently evaluating STEVAL-ISV020V1 using AN4397 and I'm not reading any voltages from both LDO outputs.Here's my setup:PV_in: 2.6-2.7 V PVBATT: 5v supercapSW1 and SW2 enabledI can confirm that the supercap is charging as STORE shows ~3.9-...
Hello Engs, How do you calculate the mission profile for the LDO40LPU33RY LDO regulator in an automotive application? Best regards
I am testing the board with a 14s Li-ion battery, but I am unable to read the cell voltages or configure any register through the GUI. I shorted the X1 and P2 power supply inputs and supplied 12 V to both. This was the only setup in which I could get...
We are currently using the L9305 IC to drive solenoid contactors in our project. The hardware configuration follows the specifications provided in the datasheet.We are able to communicate with the device via SPI and read all registers. However, we ar...
Hi,Below is the setup I'm using. An SPV1040 connected to a small 2Vmp solar panel charges two 50F supercapacitors connected in series up to Vout = 4.8V. The design is taken from the AN3319 application note of the STEVAL-ISV006V2. Currently, I have ma...
I would like to use the ACST series as an AC switch for a 90kHz AC capacitive load. Is this possible?
IC Part Number _ VNLD5300TR-E Hi Team, we are using the above IC in our design. If a short circuit occurs and the current exceeds 2 A, how long will it take time for the IC to shut down? Thanks +918882226127
I need some clarifications regarding the IC from STMicroelectronics: VN9E30FTR – 6-channel high-side driver with 24-bit SPI interface for traffic signal controller applications. In the datasheet, it is mentioned that the internally limited current i...
Could someone tell me what type of diode I have? I can't find any data.L X GP128I appreciate your help.