User Activity

Hi,In one of my applications, I require to design isolated DC-DC converter with following features:Input: 24V (Nominal)Output: 0-150V adjustable by a controller (With the help of reference voltage)Power: 70WI've tried some designs that's generated by...
Hi, I want to design AC-DC converter using VIPER26H. The suitable development board is STEVAL-ISA081V1 which is based on VIPER26L. Can someone help me to find a transformer manufacturing part no.? I want 12V 10W output.
Hi,I'm searching for UHF RFID reader IC (860-960 MHz). I found the one and only solution as "ST25RU3993". But it is NRND. So, what can I use for my new design. And is there any cheaper solution? This IC is very costly. If I ignore the cost as of now,...