cancel
Showing results for 
Search instead for 
Did you mean: 

L6920D what happens if Vin = Vout

Nickelgrass
Senior II

Hello,

what would happen if I have a fixed 5V output L6920D boost converter and the input voltage is 5V. Will it just pass through?

Thanks

3 REPLIES 3
Peter BENSCH
ST Employee

Well, the control section has a minimum off time and a maximum on time, so it cannot simply run through with a duty cycle of 100%.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

but the datasheet does state, "0.6 TO 5.5V OPERATING INPUT VOLTAGE" (my emphasis):

AndrewNeil_0-1738753614900.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Even if the data sheet shown by @Andrew Neil contains almost the same data as the current L6920DB (limit min 750mA) and L6920DC (limit min 550mA), it is out of date.

Unfortunately, I don't have an STEVAL-ISA077V1 hand to test this quickly. I am also of the opinion that the L6920D should simply switch the voltage through. During a test, the values mentioned should actually be visible at the output.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.