Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Maximum current rating of STEVAL SPIN 3201

Hi, I'm trying to use SPIN3201 to run a bldc motor and the maximum current rating of the motor that i want to use exceeds SPIN 3201 rating, although SPIN 3201 is rated for 15A i don't see whats capping the maximum rating as the MOSFETS are rated for ...

R.Ravi1 by Associate
  • 946 Views
  • 1 replies
  • 0 kudos

STC3100 at startup

Hi,I just started to use the STC3100. I can read all registers but I don’t understand how I can calculate the State of Charge at startup. I followed the application note AN3064 and apparently I need a voltage measurement to estimate the State of Char...

ACHOB.1 by Associate II
  • 2215 Views
  • 5 replies
  • 0 kudos

How can I enable spv1050 ldo's

I have an eval board steval-isv019v1. It is for boost config of spv1050. ​I connected pv yo pv input connector, a li-po battery to battery output and a 22kohm load to ldo output. I measure pv input voltage as 1.5 volts, store voltage as 3.92 volts an...

FYUCE by Associate
  • 1370 Views
  • 2 replies
  • 2 kudos

Resolved! Controlling STSPIN250

Hello,I am implementing a dc motoro control and I am a bit confused about the control of STSPIN250.I have acquired the kit "x-nucleo-ihm13a1" and I am not sure about the signal handling. I thought I could inject a PWM signal into the STSPIN250 for co...

Jhern.1 by Associate II
  • 1718 Views
  • 3 replies
  • 0 kudos

Resolved! Damaged MOSFET, urgent analysis of the damage and cause required.

Hello community,i urgently need analysis of a mosfet from st semiconductors with the cause of the damage. Can someone tell me whether an analysis and assessment of the damage as well as a possible cause for it can be carried out at ST in-house in Ger...

AWisn.1 by Associate II
  • 2591 Views
  • 4 replies
  • 0 kudos

I just purchased a STEVAL-PC009V2, but the STSpin software says my firmware is out of date. Now, the IBUUI updater tool gets stuck on switch to DFU mode.

From the UM1612 User manual, it says the IBUUI updater tool only works with Windows XP.This is 19 years old? In 19 years, no one has updated the IBUUI updater tool?How do I get the latest firmware on this evalulation board?At the very least, put the...

CBeif.1 by Associate II
  • 1099 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.