cancel
Showing results for 
Search instead for 
Did you mean: 

what are the precise timings for external flip flop involved into STNRGPF01?

NAN
Associate II

I plan to use STNRGPF01 to buil a PFC, eval board comes with 2 74HC132 package that are quit huge regarding the STNRG size.

I would prefer to use single gate and TRUE D flip flop with set reset...

knowing precise timings for Set and Reset will be a great help....

by the way ... why STN don't directly perform these PWM output? a mess to have external glue logic like these... ?

moreover at startup NAND gate output are undifened, fortunatly some capacitor are here to fix that on eval board

regards

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0