cancel
Showing results for 
Search instead for 
Did you mean: 

LED6000 use DIM as enable

Erik de Wit
Associate II

Hi all,

The LED6000 has a seperate EN and DIM line. I would like to use the dimming feature and also be able to disable the device. It seems I could use DIM only, and tie EN to VCC. Then, if I hold DIM low, the device should be disabled. As I use multiple drivers in my design, I only need 1 line per driver from the microcontroller.

Does anyone know if this is correct?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0