Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! L6206Q Power Supply Range

Hi, I am just wondering would it be ok to operate this IC with 52 to 55V supply? Hoping to use this with a 52V battery without the trouble of designing a new power supply.Clipper circuit will also be incorporated to eliminate any voltage spikes.Regar...

DLuce.1 by Associate
  • 1130 Views
  • 1 replies
  • 0 kudos

Hi, As a part of our new product, we have decided to run the product on PD capability. So, we have decided the product to be developed with two USB PD ports, so that one port can be used for Wall PD charger and other port for PD by laptop.

We have decided to use STUSB4500 for stand alone PD controller, But the main struggle is to coordinate these two PD ports and switch between them as availability.Priority is given for Wall charger PD port and the other port is used for PD when Wall c...

AV.6 by Associate II
  • 2470 Views
  • 5 replies
  • 0 kudos

Date Code Markings

Hi, where finde, and decode date of production for triac BTA12-600BW and other triacs in TO-220 package?

L6387E maximum gate drive current?

Hi,We are using a L6387E to drive two half-bridge MOSFETS of type STW20N65M5 or equivalent in a off-line DC/DC converter.The circuitry in between consists of a 10 Ohm resistor, and a diode+3.3 ohm resistor in discharge-direction, in parallel respecti...

0693W000008ydqSQAQ.gif
GAnde.1 by Associate II
  • 1518 Views
  • 1 replies
  • 0 kudos

Resolved! Battery charger ICs run from rectified AC input

Will IC such as L6924U operate with AC ripple on the power input? That is as if the power input were rectified AC with no reservoir capacitor?I posted this before but can not find the post now? Sorry for duplicating the question if it is duplicated...