Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STC3115 SOC show wrong

Hi, started using chip STC3115 in custom designed PCB. Everything is work fine, voltage and current measure good. But If I charging the battery SOC doesnt show correctly. I using it with driver from official STM site. I connected to chip 12500mA Li-p...

0693W000008zfTIQAY.png 0693W000008zfVdQAI.png
lorant124 by Associate III
  • 1317 Views
  • 1 replies
  • 0 kudos

Resolved! Shoot Through - Bootstrap Capacitance Question

I'm seeing shoot through on the coil drives for the STSPIN32F0A custom implementation in the attached schematic. The attached scope shot has these channels:CH1: 24VCH2: CoilCH3: Low Side GateCH4: High Side GateYou can see the 700ns of deadtime when t...

WSega.1 by Associate II
  • 4539 Views
  • 4 replies
  • 0 kudos

I'd like to porting software from P-NUCLEO-IHM03

I'd like to porting software from P-NUCLEO-IHM03 (NUCLEO-G431RB + X-NUCLEO-IHM16M1) to NUCLEO-G474RE+ X-NUCLEO-IHM16M1. Are there hardware differences between NUCLEO-G431RB and NUCLEO-G474RE that exclude such software porting?I installed on my PC sof...

POlcz by Associate III
  • 1068 Views
  • 2 replies
  • 1 kudos

STC3117: SOC level of Ri referred to by datasheet

For calculating the VM_CNF value the datasheet of the STC3117 gives the follwoing equation:VM_CNF = Ri * Cnom / 977.78,where Ri is the impedance of the cell.The impedance of the cell however depends on the SOC, so i wonder at which SOC the Ri is supp...

msz by Associate
  • 1573 Views
  • 3 replies
  • 0 kudos