Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We're looking to use some of the H-bridge parts such as VNH7070AY or VNHD7008/7012AY for PWM motor control and have an input usage question.

I can see that the datasheets and app notes say that the PWM input can operate at up to 20kHz PWM frequency, but I can't see anywhere anything that discusses using a PWM signal on the INA and INB inputs. Can we apply a 20kHz PWM signal to these inpu...

IWyli.1 by Associate II
  • 1371 Views
  • 2 replies
  • 0 kudos

Resolved! powerstep01_target_config generated by SPINFamily tool

when I use powerstep01_target_config generated by  SPINFamily tool on 401re the speed profile run 10 times faster that it runs on SPINFamily tool. I also change sys clock speed but no luck. please let me know if there is a solution to my problem.and...

ahagh.1 by Associate II
  • 3478 Views
  • 4 replies
  • 0 kudos

Resolved! Input Signals EVALSTDRIVE101 in ENx/INx Mode

Since I'm not allowed to work with Motor control library, I need to generate the output signals for EVALSTDRIVE101 on my own. Apparently it does not work when I put PWM signals on INx and 3.3V on ENx. (Of course I selected mode INx/ENx). From what I ...

meltabo by Associate II
  • 1959 Views
  • 3 replies
  • 0 kudos

STCMB1: output driver pins current limit

Hi, the output pins of the STCMB1 (pin 14 ,16,19) that drive the mosfets gate are protected from transient current peaks ?In the datasheet there are the current capability of the drivers (e.g pin 14 GD_PFC is capable of a 0.6 A source current and a 0...

Francis1 by Associate
  • 874 Views
  • 0 replies
  • 0 kudos

How to access function pointer for driver file

I'm using an x_nucleo_ihm03a1 powerSTEP01 module. I'm trying to understand the library ST has already made (X-CUBE_SPN3). Using ctrl+leftclick in CubeIDE, im tracing function calls to the files they were declared in. In the main.c file of the library...

ZHama.1 by Associate II
  • 2528 Views
  • 5 replies
  • 0 kudos

Resolved! How to calculate stall thresholds for a given motor?

(Finally got the powerStep01 working)I have a Vexta PK266-02A stepper motor with has a phase resistance of 3.6Ωs. I am running the driver at 18V, and I am using the SPINFamily Evaluation tool. Whenever I issue a command, I promptly get an overcurre...

Kurtnelle by Associate III
  • 1839 Views
  • 2 replies
  • 0 kudos