Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
"This kit is not a finished product and when assembled may not be resold or otherwise marketed" c2014 STMicroelectronics - All rights reserved (UM1823)
Is there a model to replace VND830LSP ?
When status of VOPRG pin is sampled by L6924D battery charger IC ? Is this sampled only from rising edge of VIN, all the time or from some other event)?Would it be ok to control VOPRG with collector of external NPN transistor (emitter of that transis...
X-NUCLEO-IHM03A1 stepper motor control board seems not available anywhere, whatever the reseller, and they have no information about a future availability. I have found no other compatible motor driver that can replace it (my motor is 48V / 9A), so t...
We have been using the STC3115AIQT in a released product, but have run into a number of rare issues relating to the SOC value. We have the STC3115AIQT connected to an STM32 STM32F091, on an I2C bus. The I2C bus is shared with several other devices (n...
We have purchased an EVLPOWERSTEP01 and a STEVALPCC009V2. We installed the SPINFamily software on our Windows10 64-bit computer and on connection it states 'The FW version is not the last, upgrade to 2.7'. The document states this is done via the IBU...
Hi, I have purchased the STEVALISN68 WA and STEVAL-ISB045, and set it up by plugging in the usb as instructed in the datasheet. But the GUI does still is unable to detect either devices. Is there something I might have missed out?
Hi.We are students working on a hardware project. We are designing based on the STEVAL-ISB68WA design and would like to know the derivations which could aid in our design(the formula for calculating the capacitor and resistance values).Is there anywh...