Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to Find MOSFET

Hi, dear. Could you please help me find the datasheet for the MOSFET with part code GF329MB, as well as other compatible MOSFETs with similar specifications?   Thank you in advance for your help! Hi, dear. Could you please help me find the datasheet ...

1000241910.jpg
manmohan by Associate
  • 363 Views
  • 1 replies
  • 0 kudos

L9780 Supporting Firmware

Hello,Does anyone have any firmware for interfacing with the L9780 wideband controller. I am planning on using a LSU 4.9 but any sensor configuration would be useful.Any information is appreciated. Thanks,

Requesting Spice Model for L9338

Hello I’m currently working on a design that uses the L9338 Quad Low-Side Driver and would like to perform circuit simulations in LT spice (or any compatible simulator). Could you please provide the SPICE model for the L9338?If it’s not available pub...

Anusree by Associate
  • 304 Views
  • 1 replies
  • 0 kudos

Resolved! STUSB4500 Variable Voltage

Hello,  Is there a way to set up the Sink PDO to take in a variable voltage? I would like to set up PDO2 5-20V 3AmpsPDO3 5-20V 5Amps  My plan is to use the Power Ok GPIOs to determine how much current I have and do some down stream current limiting. ...

mreilly by Associate
  • 640 Views
  • 1 replies
  • 0 kudos

SRK1000 usability test remarks

Last week, I have been testing SRK1000A in EVLSRK1000A-PF, in an application with 250 kHz fixed frequency flyback PWM with primary side control.1. I struggled around the gate no longer driven in CCM-mode, and even in DCM upon more than moderate load....

RMari by Associate II
  • 374 Views
  • 0 replies
  • 0 kudos

Resolved! VN9E30F: SPI Error & Fail Safe mode isnot getting clear.

Hello,I am trying to send first command from the MCU (s32k312 -NXP).I am able to send but I am getting SPI response likeAnd afterwards, no matter which SPI commands send, it always sends same response from the chip i.e. 0x610000As per the Datasheet, ...

chintantvs_0-1761305090175.png

L99LDLH32 modify Responder ID issue

Hi everyone,Good day!I'm currently working on modifying the Responder ID using CAN FD communication.I initially had a firmware running on an MCU that was capable of modifying the Responder ID. My goal now is to analyze the CAN FD communication from t...

rsiigod by Associate II
  • 1071 Views
  • 3 replies
  • 0 kudos

Resolved! STW3N170 - DC SOA

Hi ST,I am using the STW3N170 in a linear application (constant current source) where the voltage can be 1500V and current as high as 16mA - total 24W.Can you please share the DC Curve of the SOA, please include in the graph the Thermal Instability d...

STP16CPC26 flash on power up

Hi! I'm using the STP16CPC26 as an LED driver, but have a problem where all the attached LEDs initially flash when powering up. This is a problem since this is a UI with a large-ish number of LEDs and you get hit right in the face with the bright fla...

L6981CDR stops working

We have approximately fifty modules in the field that use the L6981CDR. The schematic below shows how they are connected. The L6981CDR is used (in combination with other components) to generate an output voltage of 5V. This output voltage is used to ...

OnRoute_0-1747223630430.png OnRoute_1-1747223630434.png OnRoute_2-1747223630436.png
OnRoute by Associate
  • 1175 Views
  • 3 replies
  • 0 kudos