Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Hi, I have an IC in hand which is written "HVLED01A" on it and I want to know its product number.I wonder is that same as "HVLED001A" product number or it is different IC? Thank you in advance.
hi I wanted to design a driver for the control of a 380v three-phase analog current motor, in a nutshell a classic inverter that modulates the frequency of the phases and therefore the number of revolutions of the motor. which board do you recommend?
Hello,I would grateful for some clarity on the expected bit order when writing to the configuration register of the LED1642GW.Whilst it is clearly documented that CFG-0 is the LSB, and CFG-15 is the MSB of the serialised word, it is not clear to me w...
I have a project whereby I intend to cascade 13 LED1642GWPTRs, in order to control a number of RGB LEDs.As an "in-progress-check", I have currently placed only two LED1642GWs, each as the schematic below, with SDO of the first chip connected to SDI o...