Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which IC has "HVLED01A" marking code?

Hi, I have an IC in hand which is written "HVLED01A" on it and I want to know its product number.I wonder is that same as "HVLED001A" product number or it is different IC? Thank you in advance.

MFath.2 by Associate
  • 1602 Views
  • 2 replies
  • 0 kudos

3 fase 380 v motor driver

hi I wanted to design a driver for the control of a 380v three-phase analog current motor, in a nutshell a classic inverter that modulates the frequency of the phases and therefore the number of revolutions of the motor. which board do you recommend?

SDall by Associate II
  • 2563 Views
  • 4 replies
  • 0 kudos

Resolved! LED1642GW - Endianness of Configuration Register?

Hello,I would grateful for some clarity on the expected bit order when writing to the configuration register of the LED1642GW.Whilst it is clearly documented that CFG-0 is the LSB, and CFG-15 is the MSB of the serialised word, it is not clear to me w...

GKerwood by Associate II
  • 831 Views
  • 2 replies
  • 0 kudos

Resolved! LED1642GW - No data output on SDO

I have a project whereby I intend to cascade 13 LED1642GWPTRs, in order to control a number of RGB LEDs.As an "in-progress-check", I have currently placed only two LED1642GWs, each as the schematic below, with SDO of the first chip connected to SDI o...

0693W00000KdLjAQAV.jpg
GKerwood by Associate II
  • 1909 Views
  • 3 replies
  • 0 kudos