Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AC or DC input (ultra-wide input)to DC output SMPS circuit design ?

Dear ST team,​I want to design an SMPS circuit with the following specifications:​​* Input can be either 33-265 VAC or 48-375 VDC (ultra-wide input)​​* Multiple DC outputs​1.output : 24V with 0.7 A​2.output : +10V with 0.8 A​1.output : -10V with 0.8 ...

Zaim by Associate II
  • 841 Views
  • 0 replies
  • 0 kudos

PM8804 VC high voltage set incorrect voltage level

I’ve build 5 boards using PM8804 and only one board seems to regulate the VC (Output of the internal high voltage start up regulator) according to the datasheet where the high voltage regulated drop below 6V when it detect auxiliary power detected hi...

TLy.3 by Associate
  • 832 Views
  • 0 replies
  • 0 kudos

Hello everyone, I am trying to use the PWD13F60 full bridge driver IC to drive an acoustic transducer. I am using the corresponding evaluation board for test purposes. I have a question about the IC. What exactly is the purpose of the SENSE pins?

I noticed the pads of these pins are very small. I'm a bit worried this is critical with high-current thoughput. For my application current peaks might exceed >5A for couple us. Pads like GND, VS and OUT are very large in comparison..

CGünt.1 by Associate
  • 895 Views
  • 1 replies
  • 0 kudos