Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Working on an application with IPM STGIF5CH60TS-L

Q1: It has max current rating of 8A; however, i can not find the power rating in datasheet. How to determine its power rating?Q2: How to determine the max RPM that it can drive given # of poles?Q3: it supports voltage up to 600v per datasheet. Is the...

GChen.13 by Associate
  • 1502 Views
  • 3 replies
  • 0 kudos

About specification (pulse-skipping) of STBB2

What is the state of "Pulse-skipping" in Table 6 of 5 Electrical characteristics?And please tell me the conditions for transitioning to the Pulse-skipping state.It is written on page 8 of the STBB2 data sheet.See attached file (_pulse-skipping.jpg) i...

GoToHiro by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

About specification (Ips-pwm) of STBB2

What is the value of "Ips-pwm" in Table 6 of 5 Electrical characteristics?It is written on page 8 of the STBB2 data sheet.See attached file (_Ips-pwmjpg.) in details.​Please answer in Japanese if possible.

GoToHiro by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

Does a switching regulator effect the output of a buck converter with a fixed output voltage of +5 V like the L7805?

I'm trying to design an voltage regulator on a motor control board. I want an output voltage of 5 VDC and the input voltage is 24 VDC. Because of heat production i was thinking about using a switching regulator like the L7983 followed by an L7805. Bu...

FKamm.2 by Associate II
  • 6223 Views
  • 14 replies
  • 0 kudos