Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
In my previous post I showed a fault condition using a STSPIN240 and a brushed DC motor with a supply voltage of 9V. I assumed that this issue would be resolved if I instead used the STSPIN250, as this would allow the current protection limit to be d...
I am having some trouble using the STSPIN240 brushed dc motor driver with my motor:Sparkfun ROB-16413From my calculations, the motor should not draw enough current to trigger the overcurrent/short-circuit protection.My measurement show a large spike ...
Also, the red led of IHM02A1 is On all the time .Is this normal?Thank you.
HI, the video shown that the scs001V1 can be auto select the voltage needed for the devices has plugged it in.what i see is that the eval board output the power thru the terminal block, i am curious how it will auto select the voltage needed? that is...
Pspice model is not available for this LDO LD49100PU12RY.Please can you provide the Pspice model for LD49100PU12RY.
Query above is straight forward. - Deadtime implementation options for Half Bridge config.Deadtime is to "wait for one FET to switch off" b4 turning on the other FET in the half bridge. This is to prevent shoot thru for the Power supply via the Half ...
Hello,sir/mamWe have developed the schematic as per the reference of the STREF-SCS001V1 Board.I know the STUSB4500 requires PD enable charger as its source so we have taken PD enabled adapter.I have been using STM32F072 EVM board to detect the STUSB4...
Please provide Spice model for LD49100PU12RY
Second time i am asking my issue but not a single reply from your side, Please solve my issue As soon as possible, else please tell me the procedure raised a escalation. .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.