User Activity

Hello,In the wiki I have found these lines:5.3 Non-volatile counters↑Each certificate embeds a non-volatile counter value that is checked to control anti-rollback mechanism.There are two non-volatile counters: - Trusted non-volatile counter - Non tru...
Hi, I'm trying to leverage the capability of lower words to be programmed once to one bit by bit to implement a sort of "forever growing counter", not sure if there is a proper naming for this.In the lower OTP zone, if I understood correctly, word 10...
Hello, I'm trying to leverage the MCO capability of the STM32MP1, but I don't success. I want to have LSE on MCO1 and HSE on MCO2. I'm using TFA -> uboot -> linux and I can build with Yocto or Buildroot.Which steps should be done during TFA, uboot an...
Hi,I'm trying to bring up a custom board based on STM32MP151C MPU. The design is widely taken from the devkit.I'm booting from SDCARD and bootpins are set accordingly (b101).One thing that is changing is the I2C4 pins for PMIC interface (still on I2C...
Hello all,I'm designing a custom board based on MP1 familly and I'm using the STPMIC1APQR PMIC. To validate my design, I would like to simulate it. ​Is there any SPICE (Or IBIS etc) model of the PMIC available that can allow me to progress on that po...
Kudos from