Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VN5160S-E - 28V on INPUT pin, damahing my uC

HI all,Has anyone come across their HS switch putting voltage back onto the input pin of this device which is at VCC level (28V for me) so this is then going back to my microcontroller and damaging it. In what scenario is this even possible?Here is m...

Screenshot 2023-07-17 111104.png

SOP vs HSOP

I have some EOL components with two different part numbers, but I believe they are the same.  VND600SP13TR HSOP10 and VND600SP13TR SOP10.  What is the difference between the HSOP10 and the SOP10?

danm by Associate
  • 948 Views
  • 0 replies
  • 0 kudos

L9963E

Hello!I am considering your L 993E for a new automotive BMS project. One of the biggest question marks is: why does it only have 14channels? We are aiming at 48V system but want to open for LifePo cells as well. Thats why we would need 16S /channels....

Orbiter by Senior
  • 1016 Views
  • 0 replies
  • 0 kudos

Is VNQ660SP output STATUS pin Open drain ?

Hi, the datasheet of VNQ660SP do not specify if the STATUS pin is Open Drain or not. It is more clearly defined in other chip like the VN330SP.In other word, we use many of the VNQ660SP on the same board and did connect the STATUS pin together. Is it...

LKnuc.1 by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! Devices marking

Hello, I have some doubt on part number L9942XP1TR. What the meaning for letter "RR" on top mark. Can you provide some parts mark information? Thanks Man  

Manman_0-1688538883149.png
Manman by Associate III
  • 2677 Views
  • 2 replies
  • 1 kudos

Parts marking

Hello,Is it normal for parts marking? Please find the attached photo.ThanksMan 

IMG_20230711_215608.jpg
Manman by Associate III
  • 1550 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.