cancel
Showing results for 
Search instead for 
Did you mean: 

VN750PTTR-E Date Code

igamoso
Associate III

Dear Support,

Please confirm if the DC for the part number VN750PTTR-E in the marking "235" is 2235.

Year: 2022 and Week 35.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The date codes are to be interpreted as always: YWW, which also applies to the VN750PTTR-E, which has the component marking VN750 and the line below with PT.

Since VN750PTTR-E was launched in 2004, the examples should be read as:

  • 235 = 2012 or 2022, week35

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.