User Activity

Hi everyone,I am using from STM32G4 series MCUs. In these 32G series, according to what is written in the errata sheet, there are some problems with the ADC hardware for Cut2.2 (Device Marking Y).The workaround provided doesn't work for me.I have 3 d...
Using STM32G431, I designed a controller and inverter with different pin sequences for my needs.I used ACS781 as a current sensor. I use the software of ST only in test. Apart from that, I develop my own software.In MC SDK 5.4.4 version, some correct...
The supply of the STEVAL-CTM009V1 board is shown to be up to 48 V. However, the A7986ATR writes that the A6902D13TR buck converter has a maximum supply of 38V.How does this board work at 48V?Or is the feeding range of the board written wrong?
The supply of the STEVAL-CTM009V1 board is shown to be up to 48 V. However, the A7986ATR writes that the A6902D13TR buck converter has a maximum supply of 38V.How does this board work at 48V?Or is the feeding range of the board written wrong?
Hi everyone,I recently purchased the B-G431B-ESC1 kit. I did a sensorless experiment with the ST motor control workbanch and it worked as expected. However, when I want to test with the encoder, the rotor remains locked and does not rotate after alig...