cancel
Showing results for 
Search instead for 
Did you mean: 

T2535-600G has Snubber built in? Thanks

HLuu.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @HLuu.2​, to the community!

TRIACs with the term Snubberless in the data sheet do not have a built-in snubber, but are designed to operate without an external snubber under certain conditions. The T2535-600G is also such a snubberless TRIAC.

You can find more information in this presentation.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
HLuu.2
Associate

Thanks Peter and Happy Holidays!

Hung

Peter BENSCH
ST Employee

You're welcome, happy holidays too!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.