Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPS5H100AF operating temperature?

Regarding the STPS5H100AF, the datasheet states that the storage temperature is -65 to 175°C, but there is no mention of the operating temperature.What is the operating temperature?

Ryo10 by Associate
  • 848 Views
  • 3 replies
  • 1 kudos

Resolved! Misleading statement about TS function of BQ25120A

Hi,Our development board uses BQ25120A for battery management.In the datasheet section 10.2.2.1 Default Settings, there is a statement:• If the function is not needed, connect TS to the center tab of the resistor divider between VIN and the ground.(p...

cyber_v1 by Associate III
  • 1629 Views
  • 6 replies
  • 7 kudos

STPM801 with a I2t characteristic

In our application we use the STPM801 as a switch and fuse. The fuse characteristic is, by default, very linear (except some filter/blanking times). Is it possible to give the fuse a I2t characteristic like old fashioned fuses/thermal fuses?I did exp...

JTo by Associate
  • 392 Views
  • 0 replies
  • 0 kudos

EVAL BOARD L9301 SPI COMMUNICATION

How to drive HSD and LSD pin using SPI command in EVAL BOARD L9301 and we need technical details what frame we have to send form our ECU to actuate the LSD and HSD drive and even more technical details related to this we are waiting for your immediat...

Resolved! Qi2.2 25W receiver

Hello,We see that there are Qi2.2 25W transmitters that have been certified. Is there any roadmap for Qi2.2 25W receivers?Thanks

davidalo by Associate
  • 966 Views
  • 3 replies
  • 0 kudos

Resolved! powerSTEP01 advanced current control parameters

Hello,are there any example parameters available to drive a stepper motor fast in current mode? I am using the EVLPOWERSTEP01 evaluation board with different stepper motors, e.g. Oriental PK267JDA (3.4V, 2.8A, 1.2Ohm) and Nanotec ST6018K2008 (4.8V, 2...