cancel
Showing results for 
Search instead for 
Did you mean: 

Power Delivery IC requirement for USB-C DP alt mode

yadagiri1
Associate

 

Hi I am developing new carrier board for COMe type-6 Module. Where i have a requirement of Display port to connect an external display with 5v @3A max, 9V@1.67A max. below block diagram has 

1. COMe type 6 module (Host).

2. Re-driver (MPN: TUSB1046A-DCI) for DP lines and USB lines.

3. A variable buck converter which will provide power from 12V source, for which need control signals from a PD IC.

4. We are looking a Power Delivery controller which will support the alternate mode , can you please suggest the PD IC from ST Microelectronics???

 

yadagiri1_1-1745825126536.png

 

 

 

1 REPLY 1
FBL
ST Employee

Hi @yadagiri1 

For your project, I recommend using an STM32 with an embedded UCPD peripheral, combined with a TCPP (Type-C Port Protection). This offers efficient management of USB Power Delivery and cost effective. 

Check this wiki for simplified implementation. 

Here an example using STEVAL-2STPD01 kit includes an expansion board with two Type-C ports and integrates two STPD01PUR programmable buck converters. It is paired with the NUCLEO-G071RB +TCPP02-M18. Some resources :

Our expert @NBALL may help you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL