Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can T1635-600G replace T3035H-6G?

We selected the Triac ST# T1635-600G for refrigerator project, to control the compressor (inductive loads). Tested T1635-600G, the heat is very serious when passing 16A current, even using a heat sink temperature is more than 100°C. Therefore, I want...

Margaret by Associate II
  • 1777 Views
  • 3 replies
  • 0 kudos

What is the correct way to drop voltage in circuit

 Hi Team i designed the schematic shown below for my automotive GPS Tracker Screenshot 2024-05-27 1500131355×883 62.2 KBHere i used diodes for droping the voltage main regulator D17 used for 5 to 3.8v approx.auto bat circuit D7 used as 4 - 3.8v appro...

Screenshot 2024-05-27 150013.png

STC3115 OCV offset

Hi, I would like to adjust OCV parameter in STC3115. In datasheet I see equation for calculation OCVtab value. But I don`t understand it. If I have STC3115IQT and I can set 100% SOC from 4.313 V to 4.22V.(4.22-4.313)/0.55 = 0.05 but to register I ca...

0693W00000FB6rEQAT.png 0693W00000FB6x6QAD.png
lorant124 by Associate III
  • 1376 Views
  • 1 replies
  • 0 kudos

STEF12PUR

Hello I want to use STEF12PUR (electronic for 12V) and have following question:1. What is the response time of this fuse (how fast it will trip in case of over current)?2. For me not clear difference between ILIM and ISHORT?3. If I want to set fuse f...

Battery Management System

Dear all,I am a BMS engineer looking for an automotive-grade BMS solution. Is L9961 good enough to develop an automotive-grade BMS for onboard battery pack monitoring? Do you have any other suggestions?Thank you very much.

khwuuk by Associate III
  • 1808 Views
  • 2 replies
  • 0 kudos

I2T curve of VNF1048F

Hello everybody,I am working on the I2T functionality of the VNF1048F high side switch controller with intelligent fuse protection.I have set the VOC THRS as 16.8mV & VSHC THRS as 91.9mv. Tnom is taken as 2sec. I am trying to plot the i2t curve given...

srnath_0-1716535352793.png
srnath by Associate II
  • 1178 Views
  • 0 replies
  • 1 kudos

eval L9963E board

Dear All,   I purchased the L9963e board for demonstration of the BMS systems. I installed the NI tools and opened the same and its opening.  I am unable to make a communication. I installed the FTDI driver as mentioned in the user manual in windows ...

STGIB20M60TS-L Heating

Hi there!I'm using the STM32G474E-EVAL to drive the STEVAL-IPM20B (eval board for the STGIB20M60TS-L). I'm running my motor (SM3L-084A) at 380V. Note, I've checked with the vendor about running the motor at higher voltage than quoted and there should...

thutch by Associate
  • 844 Views
  • 0 replies
  • 0 kudos