User Activity

Hi there, I have two questions on moving forward with a STUSB4710 in a 5k EAU project.  1. Do you have recommendations on a setup to program the NVM in a CM environment? Likely this involves custom firmware based on the project recommended in the NVM...
Hi there!I'm using the STM32G474E-EVAL to drive the STEVAL-IPM20B (eval board for the STGIB20M60TS-L). I'm running my motor (SM3L-084A) at 380V. Note, I've checked with the vendor about running the motor at higher voltage than quoted and there should...