STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32H747 Discovery Kit Not Debug/Programmer

Hello;I can't program and debug with the STM32H747 Discovery kit. I tried Stm32cubeProgrammer and STM32CubeIDE for this. Below are the errors I have received in both.Debug configuration screen is below;STLink Serial number appears, but I can't unders...

0690X00000AsYXWQA3.png 0690X00000AsYXgQAN.png 0690X00000AsYXqQAN.png

reading flash memory

Hi, with stm32cubeprogrammer i've read flash memory, but when i want to program the micro with the file that i've read, it says that "core is locked up". what should i do to solve this problem?

Fate1 by Associate II
  • 1782 Views
  • 3 replies
  • 0 kudos

CubeIDE External Loader

Hi everyone,We're using G474 is new MCU and want to program an external flash via STM32CubeProgrammer. However, IDE can't generate valid stldr file or I have done wrong its settings. I have set the parameters as example for atollic. CubeProgrammer do...