STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to download ELF file to a STM32L4R9 board that I could program a few weeks ago but can't now - it didn't just stop working, it got worse.

Programming my board worked fine for a long time, but then it started to fail with the error messages shown below but I could get it working again by closing the IDE (STM32CubeIDE) and unplugging the ST-Link/V2 then plug in and restart the IDE - but ...

IHodg.1 by Associate
  • 3096 Views
  • 3 replies
  • 0 kudos

Resolved! How to enter ST USART Bootloader from Code?

Im trying to jump to bootloader section from my Code. I'm trying to update the firmware over USART with the intergrated bootloader. In my application I'm using USART2 (PA2/PA3) on a STM32L431CCU6 Microcontroller running native FreeRTOS. My Code to in...

_legacyfs_online_stmicro_images_0693W00000biZdlQAE.png

STM32CubeProgrammer crashes when connecting to board.

Hello,I am following a tutorial to use AWS on my B-L475E-IOT01A board. When trying to program the board using STM32CubeProgrammer, it crashes when I click "connect" in the upper right hand corner. Sometimes it allows me to connect, but then crashes w...

CCend.2 by Associate III
  • 1594 Views
  • 0 replies
  • 0 kudos

How to change scaling or font size on Linux

Hi, StM32CubeProgrammer shows up realy tiny on my Linux laptop screen (2560:1600), please see screenshot.Something similar happened to STM32CubeMx inside the IDE, I could fix that starting the IDE withGDK_DPI_SCALE=0.5 GDK_SCALE=2 /opt/st/stm32cubeid...

0693W00000D2UZCQA3.png
CDenk.1 by Associate II
  • 4815 Views
  • 4 replies
  • 1 kudos

How internal flash of STMU575/585 can be protected from copying during firmware update at manufacturer/customer side?

We deliver encrypted image to the customer-manufacturer. After image update is performed the image is stored opened in internal flash. With RDP level set to 2 it is possible protect from jtag debugging and access. But if hacker at manufacturer side, ...

VTver.1 by Associate III
  • 2484 Views
  • 4 replies
  • 0 kudos

Unable to read device id from ROM table

Hi everyone,I have a st-link v2 with the STM32cube programmer on a windows 10 PC. My target is a ISP30301 ( nrf 518222) . If i try to connect to the target , it says "Unable to read device id from ROM table". (after the hardware reset is done) . What...

fpatr.1 by Associate
  • 5754 Views
  • 9 replies
  • 0 kudos