STM32 MPUs Embedded software and solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FFmpeg and v4l2 issue.

Hiii, i am using STM32mp257f-ev1 , in this board i installed chromium and its working properly but when i was tried to run url on chrome its cause some ffmpeg related issue like pixel format unsupported. I tried to add use_ffmpeg=true and use_v4l2=tr...

tmpfs /run full OpenStLinux

On dev board STM32MP157f-dk2, I ran application in Qt, several gauges and measurements on DSI display... Next I connected CAN device to board and when a lot of frames arrive, appear a problem with tmpfs /run full ,like below:What can I do with this ?

tmpfs.jpg
ienecode by Associate III
  • 298 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP157 and boot2Qt

Hi,I'm trying to learn programming STM32MP157 with qt library using boot2qt module.I flashed microSD card using boot2qt module, prepared and employed samlpe project from qt Creator to STM32MP157. - this works fine.Now I would like to control interfac...

ienecode by Associate III
  • 558 Views
  • 2 replies
  • 0 kudos

eMMC Flash from SD Card

Hi all, I want to flash my EMMC using sd card? Do you have any guide or useful link for this?I have used Variscite SoM before and I was able to do it using yocto_install.sh script generated from yocto.How can I do this on STM32MP13X series? Regards

STM32MP1 I2S on M4 core

Hi, I want to use the M4 core to handle all Audio DSP workI can see that MXCube allows the SAI ports to be enabled on the M4 coreBut it appears the I2S ports are not. I am Missing something hereUnfortunately the Pins I need to be  the PZ0-1-2-3 as PC...

Bkell1_0-1738121273906.png
Bkell.1 by Associate II
  • 215 Views
  • 0 replies
  • 0 kudos