User Activity

On dev board STM32MP157f-dk2, I ran application in Qt, several gauges and measurements on DSI display... Next I connected CAN device to board and when a lot of frames arrive, appear a problem with tmpfs /run full ,like below:What can I do with this ?
Moved from a previous thread. @mƎALLEmunfortunately appear next problem .CAN works grate !The display connected by MIPI DSI it goes wrong when a lot of frames in CAN interface arrive. Like the display slowed down a lot ... @xchenreading this thread ,...
Hi,I am built OpenSTLinux with below configuration: uild Configuration: BB_VERSION = "2.0.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "universal" TARGET_SYS = "arm-ostl-linux-gnueabi" MACHINE = "st...
Hi, I would like to use CAN communication on my devboard : STM32MP157f-DK2. So I prepared OS, unfortunatelly I have to flash STM32MP157c-DK2 version according with problem described below: Faulty boards out of the box  So, after run OS, I edited *.dt...
Hi,On my STm32MP157c-dk2 with openstlinux-eglfs, I configured in device tree (*.dts file) CAN and works . Now I would like to set pin PH11 as GPIO input.... Please help me how sholud looks my *.dts file, and wher in linux userspace I should find file...
Kudos from
Kudos given to