STM32 MPUs Embedded software and solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157 FMC Dual Die DTS

Hello, I am trying to interface the STM32MP157 to a dual die NAND. I have found this previous post: https://community.st.com/t5/stm32-mpus-embedded-software-and/interfacing-fmc-with-multiple-chip-selects-on-a-single-nand/m-p/301979 and I can see Linu...

Resolved! Configure kernel source code failed

Following the instruction from https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt* Configure on a build directory (different of kernel source code directory)   Here for example, build ...

tpeng.1 by Associate III
  • 1641 Views
  • 3 replies
  • 1 kudos

Watchdog Panic Debugging

Hi,on my STM32MP157C / kirkstone 5.15.145 i'm currently debugging an issue which ends up in a panic handled by OPTEE: E/TC:0 Panic 'Watchdog' at ?:0 at least i can reproduce it quickly by causing traffic on SPI (connected to a BMA280 ).  ... spi_stm3...

SimK by Associate II
  • 266 Views
  • 3 replies
  • 1 kudos

Resolved! Device serial number

Simple question:If i'm right the serial number returned by cat /sys/firmware/devicetree/base/serial-number is the UID from BSEC. Where is the code responsible for setting this value? I've seen the function get_board_serial in u-boot but it doesnt see...

allard by Senior
  • 321 Views
  • 3 replies
  • 0 kudos

Resolved! bitbake error

NOTE: Started PRServer with DBfile: /home/sharan/STM32MPU_workspace/STM32MPU-Ecosystem-v5.1.0/Distribution-Package/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, Address: 127.0.0.1:35035, PID: 9978 Loading cache: 100% | ...

Sharan by Senior II
  • 1454 Views
  • 5 replies
  • 0 kudos