STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX M33 Error

Hello, everyone! I am trying to program files generated by CubeMX(6.15.0) onto the STM32MP257F-DK.  1. Downloaded the FlashLayout_sdcard_stm32mp257f-dk-optee.tsv in the Starter Package installation folder. 2. When I ran some of the example in the rep...

2025-11-04_153251.jpg 2025-11-04_154816.jpg 2025-11-04_155204.jpg
DJung.3 by Associate II
  • 351 Views
  • 1 replies
  • 0 kudos

Resolved! Enable I2C on STM32MP257f-dk

Hello,I'm working with the STM32MP257F-DK using the Yocto Project, and I'm trying to enable I2C in my custom Device Tree.However, I’m facing an issue where the I2C controllers remain stuck because of power-domain pending states.Here is the relevant d...

BarthYer_0-1763338932999.png
BarthYer by Associate
  • 871 Views
  • 4 replies
  • 1 kudos

Resolved! About STM32MP255F GPU operation

I am porting Linux to a board that uses the STM32MP255F.I used the BSP from the STM32MP257F-DK board.For now, I was able to get the LCD panel to display, but the weston-graphical-session did not start.When I added the following line to /etc/default/w...

OKN by Associate III
  • 224 Views
  • 2 replies
  • 2 kudos