cancel
Showing results for 
Search instead for 
Did you mean: 

when will be the release of OpenSTLinux 6.0

VarunKumar
Associate II

Hi,
We are working on a product based on STM32MP157A MPU, As we thinking to update the kernel and QT version, we are looking for next OpenSTLinux 6.0 which supports scarthgap yocto and QT 6.5 LTS. When do we expect this release from ST?

Also, What will be the LTS period of krikstone, mickledore and scarthgap?

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @VarunKumar 

As far as I know, OpenSTLinux ecosystem v6.0 is planned in few weeks (I have not the exact date). I confirm it is based on Yocto Scarthgap.

I think support of Qt6.5 is already available with Ecosystem v5.1.0 : https://github.com/STMicroelectronics/meta-st-x-linux-qt/tree/v2.0.0

 

For LTS period of Yocto releases, see https://www.yoctoproject.org/development/releases/

 

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

10 REPLIES 10
PatrickF
ST Employee

Hi @VarunKumar 

As far as I know, OpenSTLinux ecosystem v6.0 is planned in few weeks (I have not the exact date). I confirm it is based on Yocto Scarthgap.

I think support of Qt6.5 is already available with Ecosystem v5.1.0 : https://github.com/STMicroelectronics/meta-st-x-linux-qt/tree/v2.0.0

 

For LTS period of Yocto releases, see https://www.yoctoproject.org/development/releases/

 

Regards.

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Thank You!

@VarunKumar 

You can use STM32-OS too, which is based on Ubuntu 24.04 LTS and using less memory compared to OpenSTLinux.

 

See my signature.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

Hi, @PatrickF 

do you have any information now about the date of release OpenSTLinux v6.0 based on Scarthgap? Is it still planned for this year? Also, is there a chance to find out what component versions will be used? I mean: tf-a, u-boot, op-tee and kernel.

 

Thanks!
Przemyslaw Pacholek

Hi,

OpenSTLinux v6.0 is planned to be released before end of this month.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Thank you!

@PatrickF 

Will it affect the kernel configuration?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

All info will be updated in wiki (which switch to v6.x while existing v5.x will go as archive)

I could already give you some info:

Kernel version will jump from 6.1 (ecosystem v5.x) to 6.6 (ecosystem v6.x) 

Yocto from 4.2 (Mickledore) to 5.0 (Scarthgap)

TF-A from 2.8 to 2.10

u-Boot from 2022.10 to 2023.10

OP-TEE from 3.19.0 to 4.0.0

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
VarunKumar
Associate II

Hi @PatrickF ,

I see that ST has released OpenSTLinux6.0. I still have few questions on QT6.5 release.

  1. I referred to https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package and observed that officially from ST it supports to only STM32MP2 boards. can this be supported if build to STM32MP157C Hardware? 
  2. Currently still ST supports only QT5. Any update that officially ST will be supporting QT6.5 by this Q4 year?

Please help with the above questions.