Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IPS160H diag pin impedance

Hi ST-Communitydoes anyone know what the off-impedance of the DIAG pin is when the chip is not powered or UVLO? There is a grey resistor to GND in the "Figure 1. Block diagram" with no description. The datasheet also states a max. leakage current in ...

fae by Associate
  • 1225 Views
  • 0 replies
  • 0 kudos

SPV1050 Battery charging in case of loading

Hello there, I am planning to design an environmental IoT sensor node and i would like to incorporate the SPV1050 IC since it covers my project needs. I did extensive reading of the datasheet and there are some things I would like to get cleared:1. d...

PPats.1 by Associate III
  • 4093 Views
  • 7 replies
  • 1 kudos

L6699 incorrect startup

Hello, I have an issue with the L6699. The controller initiates the start-up sequence but after a few pulses it stops permanently.I describe the application first:Vin=385VVout=39 to 60 VTransformer magnetization inductance Lm=127uHResonant tank induc...

Gonzalo1 by Associate
  • 1155 Views
  • 0 replies
  • 0 kudos

SMPS working on 110V but not working on 220V

Dear Community,I was desinged a SMPS for my circuit which belowed picture. Its working on 110V AC and not any problem. But when I connect it to 220V AC output voltage is going down slowly and about 1 minute later its go to shutdown. I can not find an...

Mnemonic_0-1718975747345.png
Mnemonic by Associate III
  • 973 Views
  • 0 replies
  • 0 kudos

L9963E, measuring battery AC Impedance or EIS

I'd like to use L9963E to measure the AC impedance of the battery at 1 kHz. It requires applying 100 mA current at 1 kHz to the battery and measuring the voltage at 1 kHz, probably with 10 kSample/second or more.  Is it possible? Or should I use anot...

DavidR by Associate
  • 2058 Views
  • 3 replies
  • 0 kudos

EVALSTDRIVE101 BLDC driver (sensored and sensorless)

Hello Team,  We want to use your EVALSTDRIVE101 kit to drive our BLDC motor in sensored and sensorless mode. As given in the overview this board can be integrated with any STM32 microcontroller but can you suggest which STM32 board we can buy so that...

sshin.9 by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos