Hi all, I designed a custom 5W charger around the STWBC86. I programmed the config and patch found in STSW-WBC86FWBPP to the IC using WPSTUDIO and I got it to charge my device (another custom circuit, this one using a TI BQ51050 receiver IC)... for 4...
Hi all, I'm designing a Qi charger and I'm wondering if I'll need to flash each IC in production, or if they come pre-loaded with firmware? If I have to flash them, is it done via the I²C interface? Thanks!
I'm replying here just in case someone else faces the same problem. While my schematic shows a bidirectional TVS on the ring node, I accidentally picked a unidirectional part number. The way my board was assembled prevented that node from going above...