cancel
Showing results for 
Search instead for 
Did you mean: 

Requirement of DC-DC converter

prakash1
Associate

Hi ST team,

 

I have requirement of DC-DC converter as per below :-

  1. Input voltage range: 20V-30V/1A
    Required dual output  +15V and -15V.

  2. Input voltage range:  20V-30V/1A
    Required dual output +10V and -10V.

  3. Input voltage range : 20V-30V/1A
    Required output voltage: +5V only

  4. LDO for controller: Input voltage 5V and Output voltage 3.3V

Kindly suggest for the same.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

If these are to be four different applications and therefore independent converters, only flyback converters should be considered for 1 and 2 due to the dual outputs. However, it is not usually the input current of the converters that is specified, but the output current.

The output current is also missing for request 4. Could you please specify the currents for the individual output voltages?

BTW: do you know our Online Design and Simulation tool eDesignSuite? Just click on Power Supply Design Tool > DC/DC and Start Design.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.