Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enable VIPER26K

Hi there,My question is if there is a way to enable or disable the Viper26K with for example an optocoupler.In the isolated flyback topology this is done cycle by cycle. But we want to enable/disable it in the high voltage buck configuration. Can we ...

Resolved! E-L9823 pin 21 - NC

Hi. Looking to use E-L9823 as a replacement in a legacy design.The datasheet states pin 21 is not connected. Looking to confirm it is a true "no connect" internally on the part.  On our existing PCB it will be tied to +24V. Thanks.

Resolved! Heat output of RLimit of STEF01FTR (eFuse)

If the resistance value of RLimit is set to 14Ω to 22Ω, how do you calculate the heat generation of the resistor?Is 0.1W OK for other resistors?Also, can you provide the BOM for the evaluation board (STEVAL-EFUSE01)?

[vnf1048f] K Value

I'm using the vnf1048f chipset.k value is required for current sensing, but it is not specified in the data sheet.Can you tell me what the k value is?

gj by Associate
  • 670 Views
  • 1 replies
  • 0 kudos

ESD Rattings for SCTW100N65G2AG

Hello,   I am trying to find the ESD ratings for this SCTW100N65G2AG. Usually its given in datasheet where its talking mostly about electrical stress data showing the ESD HBM and ESD  CDM, but I can't find this information in this MOSFET's data sheet...

Moby by Associate
  • 722 Views
  • 1 replies
  • 0 kudos

Resolved! DeadTime on ELVSTDRIVEG611

Hi  , I've a question regarding the EVB in the subject , in the Data brief the Deadtime , with the pot in the center , is about 700ns , that seems to me a lot for the GaN device used .In the previous version ( EVSTDRIVEG60015 ) it was 100ns with the ...

Ice_64 by Associate
  • 1290 Views
  • 1 replies
  • 1 kudos

Help finding a datasheet

Hey all,I'm trying to locate the datasheet of the following device:I think that it is a Zener, but I am not 100% sure.I've done the usual "Google" for the text, but I can't seem to find it.Thanks in advance.

ST G MEV GP416 Diode.jpg
BatuKhan by Associate
  • 950 Views
  • 1 replies
  • 0 kudos