Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-IFP015V2 CMTI test method

Hello, I noticed that the ISO8200B datasheet specifies CMTI (Common Mode Transient Immunity) performance. However, I would like to know how to actually test or evaluate the CMTI of the ISO8200B using the STEVAL-IFP015V2 evaluation board.Are there any...

STBC08 Minimum Charging Current

I have a been looking at the STBC08 to charge a very small Li Ion battery (Seiko MS-920) which accepts a very small charging current.  Is it possible to increase the size of Rprog resistor to accommodate a charge current of ~1mA?  From what I read, t...

KAlbe.1 by Associate
  • 431 Views
  • 1 replies
  • 0 kudos

STEF48H28 Telemetry and status information

Hi SirI have a few technical questions regarding STEF48H28:Could you please clarify which specific telemetry and diagnostic data can be read digitally through the PMBus interface?Are the input voltage, output current, and internal temperature accessi...

TIENHUA by Associate III
  • 711 Views
  • 0 replies
  • 1 kudos

Powerstep01 power supply manangement

Hi Guys,I'm using external 3.3V to supply permanently the powerstep01 logic and would like to supply VS (24V) only when I need the motor (I put the schematic in attachment).The problem is the logic does not work without VS.Everything works fine if VS...

Sams by Associate
  • 1291 Views
  • 2 replies
  • 0 kudos

Resolved! STUSB4710AQ1TR production programming, and discharge

Hi there, I have two questions on moving forward with a STUSB4710 in a 5k EAU project.  1. Do you have recommendations on a setup to program the NVM in a CM environment? Likely this involves custom firmware based on the project recommended in the NVM...

thutch by Associate
  • 1421 Views
  • 2 replies
  • 0 kudos

L6599A Shutdown

Hello.I'm using L6599AD without PFC.Previously, the DIS pin was connected to the delay pin and used as a shutdown.However, frequent peak current caused shutdowns.So I connected DIS pin to GROUND and made it work in HICCUP mode.However, the problem is...

JK5 by Associate II
  • 524 Views
  • 0 replies
  • 0 kudos

Resolved! IPS2050H short circuit protection

Can the IPS2050H withstand a full short circuit on the outputs?Let's say the IPS2050H output is connected to a board power connector. What happens if:1. The connector is first short circuited and then the IPS2050H is turned on.2. The IPS2050H is alre...

Fredda by Associate II
  • 3883 Views
  • 9 replies
  • 6 kudos