Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STL26NM60N now only tape and reel; alternatives?

Posted on April 24, 2017 at 12:57We are using FET STL26NM60N on a PCB that we sell. These are now only available as tape and reel, in quantities of 3000, which is 25 years' supply  for us. Can anyone suggest a direct replacement? STL23NM60ND and STL...

how to use a powerstep01

Posted on April 25, 2017 at 10:24Anybody who can teach me how to use a powerstep01 to drive the step motor?I have the demo boards and the powerstep01 works well with the demos and the download software from st.com.Now, i want to use another MCU (low...

Lin SS by Associate
  • 681 Views
  • 0 replies
  • 0 kudos

STNS01 occasionally getting hot while charging

Posted on June 01, 2016 at 13:15Hi to all, i implemented the STNS01 on a small wireless sensor. The STNS01 is charging a coin cell type LIR2440. The schematics for the battery charging part of the sensor are attached below. Usually the charging proc...

L297 stepper driver help

Posted on April 20, 2017 at 00:26Hi AllI need to put L297 stepper driver in 'wave drive mode' permanently. I connect HALf/FULL pin 19 to GND but it work in 'NORMAL DRIVE MODE' by default.I tried to connect pin 19 to low in even state and get the 'wa...

Relation of L6470H Speed Related Parameters

Posted on April 07, 2017 at 08:13Hi,      I am using L6470H with stm32f103 for past few months in our project. I have clarified the KVAL value relation with motor through online.I worked out all the commands for motor running given in the  datasheet...

I am usind LD1085 voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot with 30-50 sec. Same is the condition with 10uFcapacitor at i/p and o/p and also with 22uF at i/p and 47uFa

Posted on April 11, 2017 at 07:24I am using LD1085  voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot within  30-50 sec. Same is the condition with 10uFcapacitor at i/p a...

I am usind LD1085 voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot with 30-50 sec. Same is the condition with 10uFcapacitor at i/p and o/p and also with 22uF at i/p and 47uFa

Posted on April 11, 2017 at 07:21I am using LD1085  voltage regulator connected to a 500mA of load. When the capacitor connected is 100uF at both i/p and o/p it is becoming too hot within  30-50 sec. Same is the condition with 10uFcapacitor at i/p a...

L9907 Does Not Work

Posted on April 07, 2017 at 08:26Hi ,I followed the link http://www.st.com/content/st_com/zh/products/evaluation-tools/product-evaluation-tools/automotive-ic-eval-boards/eval-l9907.html  and imitate the L9907 schematic to create my own PCB pad ,usin...