Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM32/33/34 with shunt on load high side

Posted on June 22, 2017 at 22:39Can I connect STPM32 to high-side of a load? If I do so then the shunt probes will be on 230V and 229.9V potentials. That is not wrong yet as I will not connect current negative input (IIN1) to mains neutral. My conce...

Questions about STEVAL-3DP001V1

Posted on June 21, 2017 at 10:05Hi everyone,I have purchased a STEVAL-3DP001V1, and I'm trying to make it operate. My first question concern the header J22, i.e. the prog connector. My board came without any jumper at all. But according to the board...

Kraal by Lead
  • 744 Views
  • 0 replies
  • 0 kudos

Resolved! digital light dimmer

Posted on October 08, 2016 at 16:08hi every onei am working on the digital light dimmer. i control my ssr by stm32f1.i have big problem.i want design the circuit that protect ssr(triac) when load will be short so that ssr not damage.but  any method ...

l90mehdi by Associate II
  • 1886 Views
  • 3 replies
  • 0 kudos

L78L33CD

Posted on June 09, 2017 at 11:32THE BELOW PART IS ACTIVE OR OBSOLETE?STMicroelectronics - Online Support         L78L33CD

Sensorless FOC accuracy

Posted on June 08, 2017 at 03:40We are planning to use STM's FOC for our high-speed motor controller. I would like to know about the accuracy of STM's sensorless estimation of electrical angle compared to the ground truth. Since the Texas Instrument...

getting started with the l6384e

Posted on December 01, 2015 at 19:37Hello, I set up the following minimal circuit to get started with the l6384e high voltage half-bridge driver[1]: Vcc is 5V. And with the 100K resistor on DT/SD I measure 2.2V. Which is well above the Vdt=0.5V as g...

0690X00000605dCQAQ.png
d_hug by Associate
  • 1556 Views
  • 2 replies
  • 0 kudos