cancel
Showing results for 
Search instead for 
Did you mean: 

SPI communication problem

tobias239955_st
Associate
Posted on October 21, 2014 at 15:30

hello,

I have a EVAL6480H board and try to connect it with a Atmel Xmega. But on the SDO line is always the Byte which I send before on SDI.

Does I Need to make some initalisation before start a communication?

I choose SPI Mode 3 and a frequency of 250kHz.

Hope someone can give me advise. 

#l6480 #l6482-spi #spi-config-problem
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
xbd_119
Associate
Posted on January 24, 2016 at 05:01

Hi,

 Is it solved?

 I have meet the same issue with the board 

EVAL6482H, my MCU is the dsPIC30F5011,  i 

also checked all the SPI signals, they are all flowing the spec.

 anyone can help ?