Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STBC02 Float voltage below 4.2v ?

Posted on December 13, 2017 at 08:36Hi. I would like to set a battery float voltage to 4.1v (to extend the life of the battery). Looking at the datasheet for the li-ion battery charger STBC02, it looks like this can be adjusted but 4.2v seems to be ...

How to control Brushed DC Motors control using STSPIN32F0A?

Posted on December 13, 2017 at 06:34Hi,To serially control Brushed DC motors using STSPIN32F0A.I would like to connect a bluetooth module HC-05 through the USART1's PB6 and PB7.What are the connections I need to give for the brushed DC Motors?How ma...

STBC03 Eval Kit Manual (and Board?) Error

Posted on December 11, 2017 at 19:55In the STEVAL-ISB035V1 Manual (UM2132), the schematic and ball-out refer to the STBC02 instead of the -03. Also, on the board, both R11 (in the '02' section') and R8/ R13 (in the '03' section) are installed. This ...

STC3115: Does not start up

Posted on September 28, 2016 at 19:51Hello,We are using a STC3115 in one of our designs. The problem is that it does not start up.I read: https://github.com/st-sw/STC3115GenericDriver/wiki/STC3115-FAQIt looks like the problem is that the BATD is 'hi...

Eval6470 Driver Windows 10

Posted on December 05, 2017 at 12:51Dear forum,I'm trying to use GUI from SPINFamily Evaluation Tool 3.2 on windows 10 PC and Eval6470H-DISC R1 by USB.My computer cannot recoognize the board. Installing drivers from : - STMicroelectronics\SPINFamily...

Component selection for a 48VDC/40A BLDC

Posted on November 29, 2017 at 09:18Hi,As mentioned, input voltage is 48VDC and there is up to 40A available. I would like to be able use all this to drive our motor (custom IPM). I am free to design the driver board with 3-shunt current sensing and...

L6482: Right value of R sense, for 3A stepper motors?

Posted on August 15, 2017 at 11:49Hello,I am using 'L6482H discovery board' design example for L6482 chip, for making my own pcb board, using the same mosfets, etc.At this moment, my board runs really well with 2A stepper motors and 80 mili-ohm R se...

val_ltd by Associate II
  • 2940 Views
  • 7 replies
  • 0 kudos

SCT30N120 Intrinsic Body Diode

Posted on November 07, 2017 at 12:32Hi everyone, I am planning to use sic mosfets in inverter application(2 level or 3 level) and I searched some manufacturer and prices, I saw sct30n120 and ST says ' Very fast and robust intrinsic body diode (no ne...